Hi,
I would like to use the SDK demo (02_00_00_04) to perform static measurements.
I've generated a profile with the mmWave Demo Visualizer (2.0.0) and set the RX gain to maximum (48dB) to best see the filters contribution.
The result is in the following picture. We can clearly see the contribution of the filters on the noise (green dots, 1000 frames average).
I would like to perform the closest measurements but inside the band of the filters (that would be ~2m here). That implies to use the steepest ramp possible : 100MHz/us. However, as I am working in the 76-77GHz band, I cannot generate a profile with this value with the Visualizer. I've tried to generate one, modify the ramp value to 100, adapt the number of samples but to no avail : the radar get stuck.
What are the profile constraints for the SDK demo ?
Best regards,
Massimo