Other Parts Discussed in Thread: DCA1000EVM
Tool/software: Code Composer Studio
Hello,
I am an M.Sc researcher that has no previous experience in using DSP/ARM processors. I intend to create my own application/demos out of the board, it would be extremely helpful if I was pointed to a specific demo/project or any other resource that does a simple "hello world" program on the board, developed ground up. I would like to start by running a print statement using the DSP of the board to print "hello word".
There are too many files and lines of code present in the automotive toolbox 2.5.0 demos, which make it hard to reverse engineer the purpose of each file/code to understand what is happening. On top of that, they appear to have pre-built .bin files and GUIs that make it even harder.
My end goal would be something akin to creating a beam-forming transmission/reception scheme controlled via software embedded on the board. The board should then relay back FFT of chirp packets to the laptop, which I can analyze as needed.
To do that, I would need to know:
- What a .bin file is and what a config file is and what are the differences between them.
- How to create my own .bin file and config files to program the board to do what I need it to.
- To be able to relay back information from the board onto my laptop to process it in real time (with some delay is also acceptable)
Also note that I do not have the DCA1000EVM board.
Any information/exact resources I need to look at to go about doing this would solve my problems. If I am mistaken/misguided anywhere above, please do bring it to my notice as I am a novice and not really fluent with the board's limitations and capabilities.
Thank you.
Regards,
Sawan Singh Mahara