Hi,
We are using pplCount demo in the below folder.
C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0015_pplcount_68xx
In the demo it is not finding the slow movement of the people. But once the people are detected then it is tracking even their breathing. If i want to detect even small movement of the object (In my case people with movement like the person standing in a queue and showing little movement like turning his head moving his hand) what config changes i should do?
I read the guide C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0015_pplcount_68xx\pplcount_customization_guide.pdf and when i changed different parameters as mentioned in the document but it never improved the detection. Could any one have any suggestion?
Regards,
Senthilkumar K