This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Rogowski Coil Interfacing for Constant Current Closed Loop Feedback (With OPAMP or delta-sigma ADC)

Other Parts Discussed in Thread: TINA-TI, TIDA-00777

Hi,

This is continuation topic of below thread:

https://e2e.ti.com/support/amplifiers/f/14/p/912404/3371493

I have to update PWM Duty Cycle w.r.t for Current measurement from Rogowski Coil to achieve constant current of welding machine(s)  ?

What is the best way for Interfacing Rogowski Coil for Current measurement for High Speed Closed Loop Feedback System ( Not For Energy/Current Measurement after 50Hz or 60Hz) 

1)   With Opamp 

2)  or with delta-sigma ADC

Is there way to do simulation of Rogowski Coil  ?

Thanks in advance.. Please suggest..

--

Karan123