This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alpha,
Thank you for your question. The LM73 will connect fine to most I2C masters, provided the timing requirements are met. It is designed to be compatible with both I2C and SMBus as much as possible.
It is a very old part though. If this is a new design you may want to consider one of our newer I2C parts, such as the TMP1075 or TMP112.
Best Regards,
Brandon Fisher
Hi Brandon,
I would need an automotive grade AEC-Q100 grade2 temp sensor with alert function when temp high exceeded the programmed high limit.
Could you suggest alternative part beside LM73?
thanks.
Alpha
Hi Alpha,
Here is a complete list of our Automotive, I2C, temperature sensors. Most of them are AEC-Q100 Grade 1 or higher, which will meet your requirement. Many also have an alert function like you are describing.
I would recommend the TMP112-Q1 or TMP102-Q1 if you are planning to use a 3.3V rail. These two devices are almost the same, but the TMP112-Q1 has better accuracy.
If you are planning to use a 5V rail, consider the TMP175-Q1 or the TMP75-Q1. Again, these two devices are the same, but with the TMP175-Q1 having better accuracy.
All 4 of the recommended parts have alert pins.
Best Regards,
Brandon Fisher
Hi Brandon,
Did TI have thermal chip which temperature limit is set by resistor not by I2C.
The reason is that we want the thermal chip is always-on module to monitor the board temp even when SOC is shut down and power cycle.
thanks.
Alpha
Alpha -
There are five devices we offer which are resistor programmable and Q100 qualified.
Please see from the parametric search (narrowed down to those choices) here: