Dear all,
I would like to ask about operation range of HDC2021.
When checking the data sheet, the operating range is described as 0 to 100% as follows.
However, it is stated that 20-80% is the recommended range based on the following conditions, and it is also described as No-condencing.
From the above, is it correct to recognize that the HDC2021 cannot operate underwater?
(Is it the same for other HDC series?)
Best Regards,
Y.Ottey