This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: The echo signals are too weak in the TX beamforming example

Part Number: TIDEP-01012

Hello, I met some questions of TIDEP-01012.

I used MMWCAS-DSP-EVM  and MMWCAS-RF-EVM  and mmwave studio 2.1.1.

I put a corner reflector at about 4m in front of the boards indoors whose RCS should be very very large.

Yes the target was detected but the echo signals are too weak in my viewpoint.

The boards failed to detect other small reflectors and human body.

In addition, the results always reported a fake target at about 12m which is non-existent

because the length of the room is absolutely less than 12m.

Picture 3 is the test souce example.

Picture 1 and 2 are the actual results which I think the echo signals are too weak to be used in my applications.

I just used the default configurations in the matlab files of mmwavestudio.

Is there anything wrong?

Please help me.

Thanks.