This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP461: D- Pin is connected to GND?

Part Number: TMP461


D- is connected to GND internally? why the measured resistance between D- and Pin 6 is not zero, about 1ohm.

so if I connect D+ to D-, it have the same performance with only D+ connected to GND and D- Pin is NC?