This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: Calibrating to 0.05C (50mK) accuracy

Part Number: TMP117

Given the characteristics of the TMP117 temperature sensor, would it be realistic to expect 0.05C accuracy over the range of -5.00 C to 40.00 C if the sensor has been calibrated by a lab? If so, would you recommend a 1, 2 or 3 point calibration?

Thank you.

  • Dear Greg - 

    Welcome to the E2E Forum!  -  thanks for the post

    you can expect typically +/-0.05C accuracy output from the TMP117 from -40C to 70C, with no calibration. 

    This is in the device datasheet in section 6.5, on page 5 https://www.ti.com/lit/ds/symlink/tmp117.pdf

  • Hi Josh,

    Yes, they typically have that accuracy; however, we need guaranteed accuracy. I am hoping that between the linearity of the sensor and the calibration by a lab we would get there. Also, these are to be soldered onto a PCB which, according to page 36 of the datasheet, may introduce mechanical stress that will affect the measurement error. We are minimizing the mechanical stress by NOT soldering the thermal pad.

    Best,

    Greg

  • Hi Greg,

    It's quite difficult to improve upon the calibration in production. Most of our customers will not accept the time/cost involved with implementing such a test. If you're serious about doing this, it should be possible with 1 point calibration for the range you're interested in. The TMP117 also provides an offset register with EEPROM behind it for your use. Having said that, we can't make any guarantees beyond the datasheet specifications.

    thanks,

    ren

  • Hi Ren,

    I am in awe of what the TI engineers have been able to do with this sensor at this price point. I do not expect TI to guarantee anything beyond what is in the data sheet. I was wanting to know if the engineers thought it would be possible to calibrate the sensor to 0.05C accuracy, given the characteristics (linearity) of the sensor and you have answered that question.

    Thank you,

    Greg