This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Which board is preferable for Vitals Sign demo.

Part Number: IWR6843
Other Parts Discussed in Thread: AWR1443

Hello,

We are having AWR1443 and IWR6843. And Vitals Sign demo is available for both of these boards. So which one you suggest for Vitals Sign application?

Thanks and regards,

Vijaya Krishna

  • Dear Vijaya:

    The main differences between the AWR1443 and the IWR6843 is as follows:

    1. AWR1443 operates from 76 to 81 GHz and the IWR6843 operates at 60 to 64GHz

    2  AWR1443 is intended for automotive applications and the IWR6843 is intended for industrial applications.

    Here are the links for the datasheets for the two devices.

    AWR1443:

    https://www.ti.com/lit/ds/symlink/awr1443.pdf

    IWR6843:

    https://www.ti.com/lit/ds/symlink/iwr6843.pdf

    Since both the demo is available on both boards, then each board is suitable to run the demo. The question of which board you need comes down to your use case. Use the resources I linked above to differentiate between the two and choose which board suits your application.

    Best regards,

    Connor Desmond