This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Microwave radar chip to sense human presence at a distance of roughly 20 to 30 cm

Part Number: AWR1642


Hi Team,

I would like to get some help regarding the customer request for a microwave radar chip to sense human presence at a distance of roughly 20 to 30 cm.

The customer would need roughly 100k units so I hope you can help with the following information from the customer:

"The idea is to limit the sensing to a region of a persons head in front of the device
that is at a distant of roughly 25 cm

an angular resolution for vital sign detection of roughly <10° would be preferable
further, a distinction between the reflection of vital tissue and static object reflection would be helpful

Other questions:
I would also be interested in clarification of the following 2 aspects (if possible):
1.) is it theoritically feasible to measure the heart rate from a region of a humans face via na mmWave sensor. As far as I understand the TI-examples on the TI-Website on this subject the heart rate is usually measured from microscopic movements of a person's chest (predominantly).
(https://www.ti.com/lit/wp/spry315/spry315.pdf)

2.) How exact can the distance to a face be resolved at a distance of 25cm (since I would expect that multiple echo signals from the irregular surface of the face are received at the sensor). Is my understanding correct that the mmWaveSensor delivers a range mapping of the reflected signals?

Please let me know if you have any questions with the customer.

Regards,

Jonathan Geronga
Texas Instruments Customer Support

  • Hi,

    Unfortunately we have not performed tests for measuring the heart rate from the human face.

    The vital signs demo measures the chest displacement.

    Usually there will be several reflections from the face. However based on the angular resolution, only the strongest reflection may be detected.

    For the BOOST EVM the angular resolution in azimuth is ~15degrees.

    Experiments would have to be carried out for this use case

    thank you
    Cesar

  • Hi Cesar,

    Thank you for your response and I understand your information.
    I will now resolve this case to further close this.

    Regards,

    Jonathan