Other Parts Discussed in Thread: PGA460PSM-EVM, BOOSTXL-PGA460, MSP-EXP430F5529LP, , PGA460
Hello,
I bought a PGA460PSM-EVM evaluation board for testing.
I would like to ask you to answer a few questions.
1. Is it possible to connect the evaluation board PGA460PSM-EVM directly to a PC with SW support PGA460-Q1 EVM without the use of additional demonstration kits (BOOSTXL-PGA460 and MSP-EXP430F5529LP)?
2. Is it possible to use the sensor for measuring stationary or slow-moving objects in the range of 4cm to 60cm (max. 100cm)?
3. Which components need to be replaced for this range (Ultrasonic Sensor - Transceiver, Transformer, ...)? Can you recommend any?
4. Is the ultrasonic transducer MCUSD13A300B09RS suitable (uk.farnell.com/.../2362690)
5. Which register sensors should be changed?
Thank you, Peter.