Part Number: PGA900
Tool/software: Code Composer Studio
Cortex_M0_0: Can't Run Target CPU: (Error -1268 @ 0x1080001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
target configuration according to quick start files.
test connection right.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[Perform the SWD Mode Integrity test]-----------------------------------
This test will read the IDCODE register 100 times.
The IDCODE register value is 0x0bb11477.
The SWD Mode Integrity test has succeeded.
[End: Texas Instruments XDS2xx USB Debug Probe_0]
how can i solve this problem.
Regards