Other Parts Discussed in Thread: DCA1000EVM, , IWR1443
Hi,
I use DCA1000EVM + IWR1443BOOST, mmWaveStudio to capture adc data.
I wanna know about antenna config in mmWaveStudio.
There is a checkbox to select the Tx and Rx antenna to use in the [Static Config] and [Sensor Config] tabs.
Which PCB antenna of IWR1443 corresponds to Tx0, Tx1, Tx2, Rx0.... respectively?
In addition, can you tell me the distance between tx1 and rx4 in the figure?
Best Regards,
Konishi