Hello TI,
Been experimenting with this device and I noticed that in the installation guide it is advised to angle the device around 10-15 degrees. But say if I do not do that, and then set the elevation tilt in the GUI to -10 or -20, I still see in the GUI that the beam is formed towards a -20 angle.
Also if I were to tilt the actual device and then put the elevation tilt as -10 it's actually tilted to -20 theoretically is this correct?
What is the correct configuration? Do I tilt the device and then set the elevation tilt to 0?
Please advise.
Thanks
Kind Regards
Sagar Jaiswal