Hello,
So this is a little annoying, I searched everywhere for the cfarCfg property and the doaCfg, explaining what each number meant but couldn't find anything useful!
The pplcount customization guide has stuff about the doaCfg but doesn't explain all the numbers, and nothing about cfarCfg. As for the mmwave SDK i found cfarCfg but not doaCfg yet the numbers aren't explained properly, the numberl of sections under cfarCfg in the sdk is less than the numbers in the CFG (it doesn't say what all the numbers do)
I would appreciate it if someone could explain what the numbers mean for the doaCfg and the cfarCfg. like it was done in the pplCount customization guide e.g.
So the reason Im trying to understand this is because i've been tuning the parameters to remove ghosts, better detection when people are next to each other..but when I stop moving and stand still it doesnt detect me as a target anymore and only when I start moving, so I want to increase the sensitivity, would this be the right way to go? Below is my cfg file.