This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR6843ISK: Mismatch of the range estimation

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR1443, IWR1642

Tool/software: Code Composer Studio

Hello,

I am using High accuracy demo. I have converted the UART stream of Range Estimate and I am always getting a lower value compared to the value being shown in the High Accuracy Visualizer. When the real reading is about 2.24m, I am getting 1.66m. Is there a multiplier for the visualizer. I have earlier used IWR1443 and IWR1642 both didnt have any multipliers.

Regards,

Prudhvi Sagar