This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: LVDS output SDK issues

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1843BOOST

Hello,

we have an AWR1443Boost EVM ES3.0.

Our target would be to get the raw LVDS samples from the board.

Researching through your documentation, in the oldest SDK versions there used to be a command called

"setHSI LVDS" in the .cfg file to enable LVDS output.

This doesn't seem to be compatible with newer SDK versions, at least based on the error we get in Demo Visualizer when loading the .cfg file.


The new LVDS piloting command is called "lvdsStreamCfg", but it gives a platform incompatibility error when sent to the xwr1443.


How are we supposed to issue the command for LVDS streaming again, but with newer SDK versions?
Should we use the automatic perl conversion tool for our older .cfg file?

Which NEW .cfg command line would it end up using, though?