Other Parts Discussed in Thread: UNIFLASH
Hello,
I'd like to be able to run the unit tests in order to test current DSP chain. I noticed the mmWave SDK documentation has a chapter regarding to that called "Unit Test for Object Detection using HWA" located at `ti\datapath\dpc\objectdetection\objdethwa\test\testdata`.
- If I use the IWR6843ISK-ODS device, which bin files should I use for tests - xwr68xx_aopevm_xxx_data_path_test_config.bin or xwr68xx_stdevm_dss_xxx_path_test_config.bin ?
- What is the procedure on how to run the bin files?
- Do I flash the bin files first using Uniflash? Both mss and dss?
- Do I need to provide some CFG file in order to run the tests? Could you provide an example of subframe/scene configuration? Or how do I start running them?
- How do I obtain the results? Are they sent to the serial port?
Would be great to get the clarifications on how the whole procedure is supposed to be run.
Thank you.
Regards,
Victoria