This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM, MMWCAS-RF-EVM, Do I need these Boards

Other Parts Discussed in Thread: MMWCAS-RF-EVM, IWR6843, AWR1843BOOST, MMWCAS-DSP-EVM, AWR1843

Hello everyone,

I am working in a lab which is trying to do mmWave imaging using the TI evaluation boards. Currently, we have the DCA1000, AWR1843Boost, and IWR6843Boost and have used these to do imaging. At this point in the research we are trying to image with multiple boards simultaneously as a way to improve the image quality by having more TX and RX antennas. It is important that for imaging we are able to turn each TX channel on and off individually while recording on all RX channels. I know we can do this on the AWR1843 Boost and IWR6843 Boost individually, when paired with the DCA1000 but I wanted to ensure this can also be done for the MMWCAS-DSP-EVM and MMWCAS-RF-EVM. I also wanted to see if there was any possible way to use the 3 boards my lab already has (DCA1000,AWR1843,IWR6843) to record data simultaneously as this would provide us with another option to improve image quality without needing to buy additional boards

Thank You,

Cole Harlow