Hi,
I have been experimenting with the Area scanner demo provided with the mmWave industrial toolkit. When the person moved too close (<1m) to the device, false positives appeared, i.e.- Instead of the one person, it showed 2-5 moving objects at the same time. Is there any way to overcome this issue? I have been using the "area_scanner_68xx_AOP.cfg" file to configure the device.
Also, how do I disable static objects showing up on the GUI via the same configuration file?