Other Parts Discussed in Thread: HDC2022,
Greetings. I am interested in both the HDC2021 and HDC2022 for a refrigerated compartment application that requires humidity monitoring. Our nominal ambient will be between 2°C-8°C during normal operation. Humidity will be near or at condensing.
Since we have a condensing environment, I like the HDC2022 with the IP67 protective cover, however I may also need to conformal coat the PCA where this sensor will be installed. For that reason I also see the advantage of the HDC2021 with the protective tape.
Which would be better? Are there recommendations for a protective tape or cover for the HDC2022 for masking purposes?
Best Regards, Charlie