This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: flash the cpfromProgrammer.bin into the IWR6843 HS device

Part Number: IWR6843
Other Parts Discussed in Thread: AWR1642, IWR1642, AWR1843, IWR1843

Customer is currently trying to flash the cpfromProgrammer.bin into the IWR6843 HS device and run it in order to burn the custom key. But they got no response from the serial port after the program was flashed.

From the release note of mmwave_secdev_02_00_00_02. It only supports the following devices:

AWR1642_HS ES 2.0
IWR1642_HS ES 2.0
AWR1843_HS ES 1.0
IWR1843_HS ES 1.0

Does the mmwave_secdev_02_00_00_02 package support the IWR6843 HS device? If not, is there an alternative package?

Thanks,
Nick