When I ran DataCapertureDemo_xWR.lua after connecting AWR1642BOOST(+DCA1000EVM), the firmware downloading froze at 0% and couldn't proceed. The GUI status is show in following pic.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I ran DataCapertureDemo_xWR.lua after connecting AWR1642BOOST(+DCA1000EVM), the firmware downloading froze at 0% and couldn't proceed. The GUI status is show in following pic.

Hello,
As I can see from your screenshot, the BSS FW version is 0.0.0.0, which is leading to this error.
Did you download the Firmware again after RF power up? For running this script, you just have to connect the boards to your pc. No further action is required on studio.
Regards,
Ishita