This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3004: OPT3004 – IR Rejection question

Part Number: OPT3004

We Irradiate OPT3004 with the customer's IR led. We can measure a 20x lux. According to the datasheet, IR filtering should reach 99%. Since the IR LED has visible infrared light. Does it mean that the wavelength is lower than 700 nm?

In this case, is it a reasonable result to get this lux?

 

BR,

Gary