Hi,
With the default device configuration, all the faults are enabled (not masked) and I want to keep it that way. Consider, the device reports faults that disable exciter and enters the FAULT state.
If it is required to re-enable the exciter using the override bits (ENEXTUV, ENINFAULT, ENBISTF, or ENIOFAULT), will it take effect in FAULT state?
How to safely switch-on the exciter and test for the presence of faults?
Regards, Vijay