Other Parts Discussed in Thread: TUSS4470, PGA460, TDC1000
HELLO !
I'm using a tranducer 40khz, but i got nothing out of the COMPIN and STOP
when I visualized with the oscilloscope
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HELLO !
I'm using a tranducer 40khz, but i got nothing out of the COMPIN and STOP
when I visualized with the oscilloscope
Hi Hassan,
If you are using a 40kHz transducer, I suspect you are trying to make an ultrasonic measurement through air. If this is the case, I do not recommend the TDC1000 because it is designed primarily for liquid level sensing and concentration measurements in small containers/tanks. Instead, I recommend that you consider the PGA460 or TUSS4470. You can find more information and a comparison of these two ultrasonic devices on the Ultrasonic E2E FAQ here: https://e2e.ti.com/support/sensors/f/1023/t/748143
If you want to continue using the TDC1000:
Hi,
Yes i'm using an external clock source and also i increased my PGA gain to a maximum level.
What i wondering is how can i configure the external bandpass filter ? It's that i configure in the GUI or I need some modifications with the electronic circuit ?
Hassa,
The external bandpass filter must be modified as an electronic circuit. The TDC1000 device does not integrate any of the bandpass functionality, so there are no software settings for the BPF. See section "8.3.5 Receiver Filters" of the TDC1000 datasheet for details on the bandpass filter components. The aforementioned TINA circuit I linked to in my last post is a helpful tool to help you see the component impact on the bandpass filter in the frequency domain.