Other Parts Discussed in Thread: IWR1443, IWR1642, AWR2243, IWR1843, IWR6843AOPEVM, IWR6843
I am aware of some statements related to products after checking in the forum. May I list some of them and have them verificated?
S1) AWR series fits some road/car regulation with more strict working conditions, while no obvious performance gap is found when compared to the same product number in IWR series.
S2) IWR1443 and IWR 1843 has 3 TX, which enable them to form 3-D detections.
S3) IWR1642 and IWR 1843 has a DSP on chip, which enables them to do some clustering and tracking algorithm. As a result, the TLV list can be generated after detection.
And here are some more specific questions related to my research. Could you please give me some advice on device selection(which part number suits the best)?
Q1) May I know that is there any improvement in resolution or detect object numbers for AWR2243 single-chip test board(boost) compared to xWR1443? I have seen some difference in ADC sampling rate or Interface using the compare function on TI website. And I also know that AWR 2243 chip can be used for a cascade design. May I know if there is some more difference that I should notice?
Q2) I am tending to use IWR1843. May I know if I can understand as that xWR1843 combines the advantage of xWR1443 and xWR1642. Since I am working on object tracking, I am wondering if there is any drawbacks to use xWR1843 instead of xWR1642? Is it a wise choise to use xWR1843 for short range(0.5~10 meters) multi object tracking?
Q3) I am currently working on object tracking using ROS Melodic on ubuntu 18.04. I have found some useful code IN "Inductrial Toolbox 4.4.1/Labs/Robotics/ROS Point Cloud Visualizer". It suggects using IWR6843AOPEVM. Since I have tried some older vision on IWR 14443 BOOST and worked well. May I know if I can compile and run it in ROS when connected to a IWR1843/AWR2243 after some minor revision? In other words, does the data_port of IWR1843/AWR2243 output similiar data stream as IWR1443?