This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/AWR1843BOOST: Out-of-board demo can't work

Part Number: AWR1843BOOST


Tool/software: TI C/C++ Compiler

I'm using the AWR1843BOOST demo board,and my SDK version is 03_04_00_03。My configurations are as follow(profiles_2d.cfg)
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 77 7 3 39 0 0 100 1 256 7200 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 32 0 100 1 0
guiMonitor -1 1 1 1 0 0 1
cfarCfg -1 0 2 8 4 3 0 15.0 0
cfarCfg -1 1 0 4 2 3 1 15.0 0
multiObjBeamForming -1 1 0.5
calibDcRangeSig -1 0 -5 8 256
clutterRemoval -1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1. 0.2
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0.25 8.64
cfarFovCfg -1 1 -10.59 10.59
extendedMaxVelocity -1 0
CQRxSatMonitor 0 3 11 121 0
CQSigImgMonitor 0 127 8
analogMonitor 0 0
lvdsStreamCfg -1 0 0 0
sensorStart
But after sensorStart,the Application UART Port doesn't print anything. And the board seems jump to a reset state.
I also used mmw demo visualizer,but the gui doesn't show anything either.
BTW,my power supply is a 5V 3A power supply,and I used 2 different AWR1843BOOST board,everything is the same.
Is there any suggestion?