Hi!
Thank you for advising me:
- A prime photodiode which has a low capacity (1pF), a good response time, and which can detect lights in the wavelength range 350 - 1100nm (visible + infrared).
- A second photodiode which has exactly the same characteristics as the first photodiode (capacity, dark current, response time, ...), but which only detects lights in the visible light range (thus eliminating infrared). If this second photodiode does not exist, thank you for offering me an anti-infrared filter that I can place above the first photodiode to eliminate the infrared.