This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: The alternate sequence of the two frames is inconsistent

Part Number: AWR2243
Other Parts Discussed in Thread: DCA1000EVM

Hi,

Under the advanced frame using TXBF mode, two sub-frames are configured. The first sub-frame has a frame cycle of 500ms and the second sub-frame has a frame cycle of 100ms.At run time, it is found that all 5 consecutive frames are the first sub-frame, then the sixth is the second sub-frame, and so on.But after I configured the frame cycles of the two subframes for the same time, the two subframes alternated at run time.Are there any areas that affect sub-frame alternation?

thanks,

joe