Other Parts Discussed in Thread: AWR1443
Now I have AWR1443+DAC1000. The AWR 1443 has two working mode, namely TDM and BPM. The following figures show the configuration procedure of BPM. I want to know whether the steps are correct and if the steps are wrong, please let me know. Thank you.
1 In Chirp tab, set the Start Chirp for Cfg and End Chirp for Cfg to 0 and enable TX0 and TX2.
2 In Chirp tab, set the Start Chirp for Cfg and End Chirp for Cfg to 1 and enable TX0 and TX2.
3 In BPM Chirp Config tab, set the Start index and End index to 0, set the TX0 BPM Val and TX2 BPM Val to 0.
4 In BPM Chirp Config tab, set the Start index and End index to 1, set the TX0 BPM Val to 0 and set the TX2 BPM Val to 1.
5 In Frame tab, set the Start Chirp TX to 0 and End Chirp TX to 1.