This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000EVM: Timeout Error! System disconnected

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR2243, AWR1243

Tried to bring up AWR2243 boost with DCA1000EVM capture card, and got the following errors.

I already tried the following to try to solve the issue based on the previously posted related threads, but neither worked.

1. updated to FPGA firmware version to 2.8, which is the latest

2. turned off the windows firewall

But the same DCMDCA1000EVM card and same setting worked well with AWR1243 boost. Seems that the only difference between these two boost boards is AWR2243 boost is using mmwave studio 3.0 (second generation).

Any clue what extra can be done to solve this issue?

[17:18:17] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[17:18:17] [RadarAPI]: Status: Passed
[17:18:17] SelectCaptureDevice Success
[17:18:17] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
[17:18:17] [RadarAPI]: Sending fpga command to DCA1000
[17:18:27] [RadarAPI]:
[17:18:27] FPGA Configuration :
[17:18:27] Timeout Error! System disconnected
[17:18:27] [RadarAPI]: Sending fpga_version command to DCA1000
[17:18:37] [RadarAPI]:
[17:18:37]
[17:18:37] Unable to read FPGA Version. [error -5]
[17:18:37]
[17:18:37] CaptureCardConfig_EthInit Success
[17:18:37] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 0)
[17:18:37] [RadarAPI]: Sending fpga command to DCA1000
[17:18:47] [RadarAPI]:
[17:18:47] FPGA Configuration :
[17:18:47] Timeout Error! System disconnected
[17:18:47] CaptureCardConfig_Mode Success
[17:18:47] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[17:18:47] [RadarAPI]: Sending fpga command to DCA1000
[17:18:57] [RadarAPI]:
[17:18:57] FPGA Configuration :
[17:18:57] Timeout Error! System disconnected
[17:18:57] [RadarAPI]: Sending record command to DCA1000
[17:19:07] [RadarAPI]:
[17:19:07] Configure Record :
[17:19:07] Timeout Error! System disconnected
[17:19:07] CaptureCardConfig_PacketDelay failure
[17:19:07] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_03_00_00_07\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[17:19:07] [RadarAPI]: Sending start_record command to DCA1000
[17:19:07] [RadarAPI]: Status: Passed
[17:19:09] [RadarAPI]: ar1.StartFrame()
[17:19:09] [RadarAPI]: Status: Passed
[17:19:09] Frame start async event received!
[17:19:10] [RadarAPI]: Frame Ended
[17:19:10] Frame End async event received!
[17:19:59] Please wait for a few seconds for matlab post processing .....!!!!
[17:19:59] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_03_00_00_07\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[17:19:59] [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 8
[17:20:09]
[17:20:09] ***Script completed successfully.***