This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243: GPIO (I2C Address).

Part Number: AWR2243

Hello support team.

I want to clarify AWR2243 GPIO(I2C) pins usecase.

From AWR2243(p), Both SPI and I2C functional mode are supported.

But I believe that GPIO[0-2] pins are used for I2C address selecting.

 

So, if customer will use I2C functional mode, I would like confirm (as double-check) if GPIO[0-2] pins cannot be used for general purpose I/O.

Or can GPIO[0-2] be used for general purpose pins when I2C is not communicating even though I2C functional mode is selected?

If customer will use SPI functional mode, GPIO[0-2] can be used for original general purpose pins.

 

Br

KORO