Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843
Hello,
I was trying to download firmware over SPI but got the error code -8 when booting mmwavelink_example.exe by following all steps required in documents mentioned in the link.
What does it mean and how can I resolve it? The device used is the combination of PC+ICBOOST+IWR6843-ODS (wihout Flash), and please see the attach for the detailed configuration and log files.
Thanks.
BOARDS:
IWR6843ODS,
MMWAVEICBOOST,
ICBOOST Dial - code switch configuration:
s1.1 off
s1.2 on
s1.3 off
s1.4 on
s1.5 off
s1.6 on
s1.7 on
s1.8 off
s1.9 off
s1.10 on
s1.11 on
s1.12 on
ICBOOST FTDI_USP port connect to PC with usb cable.
[SOP2, SOP1, SOP0]->[0,0,1]
ERROR:
================= mmWaveLink Example Application ====================
====================== SPI Mode of Operation ======================
Device map 1 : SOP 4 mode successful
Device map 1 : Device reset successful
rlDeviceEnable Callback is called by mmWaveLink for Device Index [0]
mmWave Device Power on failed for deviceMap 1 with error -8
=========== mmWaveLink Example Application execution Failed ===========
trace.txt:
[12:29:47:547]: rlsOpenGenericGpioIf: Got 4 devices connected
[12:29:47:953]: rlsOpenBoardControlIf: Got 4 devices connected
[12:29:48:073]: [VER] mmWaveLink Studio Version: 1.1.5.4.22.11.18
[12:29:48:450]: rlsFindAndOpenDevice: Got 4 devices connected
[12:29:48:468]: SPI port opened (DeviceNum=0)
[12:29:48:484]: IRQ & I2C port opened (DeviceNum=1)
[12:29:48:558]: FTDI Open Successful
[12:29:48:558]: Enable Device
[12:29:48:559]: Device [0] Host IRQ High
[12:29:48:559]: Device [0] [WR]0x5678 0x8765 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF
[12:29:48:563]: Device [0] Host IRQ Low
[12:29:48:565]: Device [0] [RD]0xDCBA 0xABCD
[12:29:48:566]: Device [0] [RD]0xA036 0x0026 0x000C 0x0000 0x0001 0x5F96
[12:29:48:569]: Device [0] [RD]0x5000 0x0018 0x1D06 0x0006 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000
[12:29:48:569]: Device [0] [RD]0xF8D9