HI
There are some questions about the power tree on EVM IWR6843ISK-ODS confused me, it is about the 3.3V power supply. PMIC output the PMIC_3V3 power rail, it is divided into two 3.3V power domains,
One is VCC_3V3 , this power domain is connected to QSFPI,TEMPERATURE SENSOR, CURRENT SENSOR, EEPROM, TS3A5018RSVR and so on.
The other is PMICOUT_3V3 , which is connected to UART SELECTION ,USB to UART and so on.
I wonder what is the purpose of this solution? Can I conbine these two 3.3V power domains to one?
Regards
,