This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Gigabit Ethernet interface requirement.

Part Number: DCA1000EVM

I have spent some time empirically discovering that the DCA1000EVM's Ethernet interface only works when connected at 1 Gbps.  That is, when connected to a 100 Mbps Ethernet port, it will not even respond to ARP messages.

I found this question: "DCA1000EVM: mmwave Studio : FPGA version not read, Ethernet Cable Not Connected, ADC Data Capture not working" which mentions in passing that a GigE adapter is required "as DCA1000 EVM supports up to 600 Mbps" but its top speed should not affect its ability to communicate slower.

Can you confirm this is a true requirement and, if so, point me (and future folk) at the relevant documentation?  If it's not a true requirement, can you suggest what I might be doing wrong otherwise?

It's certainly the first time I've encountered a device that behaves this way.