Other Parts Discussed in Thread: UNIFLASH, , , AWR1243
Hi there,
I'm trying to use Uniflash 6.1.0 to program the SFLASH connected to an AWR2243 on a custom board. The custom board was originally designed for the AWR1243p. I'm attempting to program the SFLASH with xwr22xx_metaImage.bin from mmwave_dfp_02_01_05_03. I'm following the same procedure that worked for us on other boards where we populated AWR1243p instead (except I'm selecting AWR2243 in the "Choose your Device" section). SOP[2:0] is set to 101. Here is the log from Uniflash when I attempt to load the meta image:
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Initialization complete.
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Flashing process starting...
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Connecting to COM Port COM10...
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Reset connection to device
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Set break signal
[7/30/2020, 1:27:24 PM] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[7/30/2020, 1:27:25 PM] [ERROR] Cortex_R4_0: Internal Error: Unknown device type. Cannot proceed. Exiting...
[7/30/2020, 1:27:25 PM] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[7/30/2020, 1:27:25 PM] [INFO] Cortex_R4_0: Instance deinitialized
Any thoughts on what might be going wrong here? Is the procedure different when you're using Uniflash with an AWR2243 part? Or does Uniflash 6.1.0 not support these parts yet?
Thanks,
Kyle