Other Parts Discussed in Thread: MMWCAS-RF-EVM
Hi TI
Hope you can help us settle an issue we have with our radar based on your XA1243FPBGABL chip.
The radar is designed using two of the mentioned chip in a cascaded master-slave-configuration.
I'm attaching a block diagram, but as you can see it follows SWRA574B.
We are not performing MIMO or beamforming with our Tx-antennas, however we would like to do a Tx-scanning scenario.
Due to antenna design and layout issues on the board we could only fit out Tx antenna configuration as you can see in the block diagram, i.e. the first antenna is attached to master Tx1-pin, the second antenna to slave Tx2-pin and the third antenna to slave Tx3-pin.
The second slide show our wanted Tx-scanning scenario: The first frame (containing 512 chirps) should be transmitted with the manster antenna Tx1, the second frame with the Tx2-slave antenna and the third frame with the Tx3-slave antenna....and then start over again according to the chart. I.e. each frame looks exaktly the same, but transmitted from different antennas.
We got everything working using only the master Tx1-antenna for all frames, but...my question is, can we configure the chips to do a scanning scenario according to my chart? And if so can you guide us within the Radar Interface Control-doc? Are you doing anything similar with some example-code for your cascaded eval board, MMWCAS-RF-EVM?
Best regards
Henric