Other Parts Discussed in Thread: IWR1843, , IWR6843
Hi,
I am doing some experiments using traffic_monitoring lab in mmwave_industrial_toolbox_4_4_0.
What I did:
1. Run traffic_monitoring lab.
2. Start walking in front of the radar from 0m to 40m.
FW: 18xx_68xx_traffic_monitoring\prebuilt_binaries\traffic_monitoring_18xx_demo.bin
config: 18xx_68xx_traffic_monitoring\chirp_configs\18xx_traffic_monitoring_70m_MIMO_3D.cfg
Please see the point cloud data attached below. This shows all the point cloud data over the time from this person starts walking until he stops.
As you can see, the elevation value is slightly wrong. I expected it to be 0 degree but actually is is around 10 degree.
Why is the elevation value is wrong by 10 degree?
Best regards,
Fields