This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1642BOOST: AWR1642 BOOST

Part Number: AWR1642BOOST

Tool/software: Code Composer Studio

 

 I have tried flashing the bin file for CAN sample code that i have loaded form the automotive toolbox lab005  in AWR1642 BOOST. It successfully flashed and when i tried to view it on the CAN visualizer GUI.It seems that the data is coming but it stops after some time and also its not showing any point cloud in the plot. Can you help me with the issue. I am using the PCAN USB FD by Peak system.

BR

Sreenath

  • Hello Sreenath,

    I hope you are using default application binary with AWR1642BOOST and followed the instruction in the user guide provided.

    Did you connect CCS and check the status of application? Is it still running and streaming object results out over CAN interface.?

    CAN Visualizer is built for reference only and it may be due to version mismatch with you PCAN dongle.

    PCAN visualizer is built with pcan-basic.zip file, you can get the source code from there and debug further in the GUI.

     

    Regards,

    Jitendrra