This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA302: Enob measurement

Expert 1190 points
Part Number: PGA302

hello, to determiner the ENOB item 3. states "Connect 5-KΩ, Zero TC bridge to the pressure input pins device with near zero differential voltage"

Can four 5K resistors configured as a bridge be substituted?

thanks