This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2080: is it possible to read the temperature and humidity values (0x00-0x03) regardless of DRDY/INT?

Part Number: HDC2080


Hi Team
My customer is planning to use the Auto Measurement Mode (AMM) shown in p.25 of datasheet to automatically acquire temperature and humidity at a 5Hz setting. 
In this case, is it possible to read the temperature and humidity values (0x00-0x03) regardless of DRDY/INT?

The intention of the question is
The time TEMP_CT (Conversion-time) required to acquire temperature and humidity is specified on p.5.
I am concerned that if the values are read during this acquisition time, the temperature and humidity values will change.
Is it okay to think that you can always read the value obtained last time?