This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: hardware trigger with frame period in framecfg

Part Number: DCA1000EVM


Hi,

If I set the frame period to 10 instead of 1 in framecfg in mmwave studio and I also use hardware trigger. What will happened when only one pulse input to sync_in?

Will it only start one frame or it will start 10 frames based on the frame period setting in framecfg?