This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Target detection algorithm & real-time streaming

Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: MMWCAS-RF-EVM, AWR2243, AWR1243

Hello!

We would like to use the MMWCAS-DSP-EVM board and cascade radar (MMWCAS-RF-EVM) to stream target detections over Ethernet in real-time.

Is it possible to run a target detection algorithm for the cascade radar on the DSP board? If so, is there any existing TI code that could be used for this purpose?

Is it possible to stream the output of such an algorithm using the Ethernet port on the DSP? Again, is there existing code for this purpose?

Thank you

  • live streaming of target detection and heatmap : please refer to PROCESSOR_SDK_RADAR_03_08_00_00

    there are some information for running program in TDA2x platform.

    However, the documents are not clear. How to generate the SD Image? The compile of the cascade example is done. 

    furthermore, the vision sdk is used for awr1243. Is the vision sdk updated for awr2243?

    Could someone give a detailed document to show the procedure where the live streaming of targets and heatmap by using Dsp EVM + Cascade RF EVM?

    Thanks 

    Kang

  • Hi,

    Unfortunately the vision SDK does not support AWR2243 cascade imaging kit.

    What you are trying to achieve is possible but it is not currently supported on AWR2243.

    You would have to rely on community forum support.

    Thank you

    Cesar

  • Understood, thank you both for the answers.