Part Number: TDC7200
Other Parts Discussed in Thread: TDC1000
Good morning.
I want to make TOF measurements on a pulse train, so that the first pulse should be treated as START and the rest as STOPs.
To ensure good timming, I was thinking of using a multiplexer and use the TRIGGER output as select bit. This way, when the device is ready to measure and TRIGGER is set high, the train is at the START pin. After the first (START) pulse, TRIGGER is set low, multiplexer changes its output pin and the rest of pulses in the train would be at the STOP pin.
I'm aware of the minimum 5ns from TRIGGER rising edge to the START rising edge. But I cannot find any information referring the time from START falling edge at its end and the TRIGGER falling edge (when TDC resets the pin). How much time would it be? Or could TDC reset TRIGGER before START pulse finishes? In that case, part of the START pulse will be seen at the STOP pin, and I don't want this at all.