Hello experts, I would like to ask if there is a way to reduce the power consumption to the minimum and if you have tested or calculated it. We are using a custom board based in the IWR684ISK, but with the minimum components and a low power consumption host MCU, so the principal concern is the power consumption of the IWR6843 IC itself, we have measured up to 4W when the BOOST board is working with the IWR6843ISK boards are connected but we believe there is much power being used for the host board and other ICs in the DEV board too.
Do you have a paper that can give us guidance how to optimize the configuration and operation to have the minimum consumption?
I Thank you in advance for any possible help in this situation.
Tomas Alarcon