This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5032: Asking for the hall sensor DRV5032 design suggestion

Part Number: DRV5032


Hi team,

If customer will overlap DRV5032FA & DRV5032FD in the board layout (one of the two to mount on the board), could customer connect both of pin3 together?


BR,
SHH

  • Hi SHH,

    For the FD version this will be OUT2 so you can use this pin as you like in your application, for the FA version this is a NC pin meaning there is no internal bond wire. So if you were to just replace the FD version with the FA version in the same layout that would be ok.