This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: Sensing distance, resolution and coil shape

Part Number: LDC1612

Hi,

By Using the LDC1612, I want to measure the target distance from minimum 0cm to maximum 8cm with 1mm accuracy.

The coil area can be 8 cm square or 12 cm wide and 8 cm long rectangular shape.
The target can be made with a steel plate or copper.

I have the following questions about this.

1. Is this enough sensing distance considering the coil size?
2. Does the thickness of the steel plate affect the distance?
3. I think you do not provide a design option in a rectangular shape, so would I just stretch the square shape to the side?

Thank you,

  • Hi Key,

    Thanks for reaching out, a rectangular shaped sensing coil is typically used for linear position measurement along a track. Its not clear to me in what axis your target will be moving. You can use the design calculator in the product folder linked below with the given distances and sensor shape to calculate you required sensor design to give you best results in your application.

    https://www.ti.com/product/LDC1612-Q1

    1. Is this enough sensing distance considering the coil size?

    • This can be calculated in the excel design calculator.

    2. Does the thickness of the steel plate affect the distance?

    • Yes, recommendation is to have at least 3 skin depths target thickness for a good LDC measurement. This can be calculated based on material type in "SkinDepth" tab of the excel calculator. Further explained in section "1.2.2 Skin Effect" of the Sensor design file linked below.

    3. I think you do not provide a design option in a rectangular shape, so would I just stretch the square shape to the side?