This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue when trying to postprocess data from test source capture

Part Number: MMWCAS-RF-EVM

Hello,

I am facing an issue with the MMWCAS-RF-EVM i have configure the board with Cascade_Configuration_TestSource.lua using the xwr22xx_metaImage.bin

Yhe script simulate 4 objects, one for each device object at 5 m with x = 4m and y = 3m for device 1, x = 3m and y = 4m for device 2, x = 12m and y = 5m for device 3, x = 5m and y = 12m for device 4.

But when i start the mmwave studio post process, I don't understand the following result.

Thanks,

Vincent